Device Driver & Libraries
Device Driver & Libraries 子类别
HX3 Rev. *C and *D silicon of USB 3.0 Hub Controllers passes USB-IF compliance (TID#330000060) with internal ROM firmware. Customers can save BOM by eliminating the EEPROM. Customers using Rev. *C Silicon and choosing to boot from an external EEPROM must use the Version B5 or B7 firmware. Customers using Rev. *D Silicon and choosing to boot from an external EEPROM must use the Version B7 firmware.
The method of identification of the HX3 Rev *D Silicon and earlier Silicon is included in the Version B7 - Release Notes.
Version B5 or B7 should not be used with the HX3 Rev *A Silicon. To pass USB-IF certification with Rev *A Silicon, customers are required to use Infineon Version B3 firmware.
All versions of HX3 firmware needs to be downloaded to HX3 using either an I2C EEPROM or an external I2C master. If an external EEPROM is used, Cypress provided Blaster Plus software tool can be used to program the EEPROM. Procedure to download firmware to EEPROM is provided at - Downloading Firmware for HX3 - KBA91657.