PSOC™ 4 Die Temperature
综述
General Description
The Die Temperature component provides access to the analog signal whose voltage represents the temperature of the die. It also provides the API needed to convert the digital voltage representation of that analog signal to a temperature. This component does not provide the mechanism to convert the analog voltage to a digital value. That must be done in the design by connecting the signal to the ADC in the device and sampling the voltage.
- Typical measured accuracy of +/- 1 ºC
- Valid operating range from –40 °C to +85 °C
支持