Infineon: 1st supplier of magnetic angle sensors to achieve the highest automotive functional safety grade with only one sensor chip

Jun 22, 2018 | Market News

Munich, Germany – 22 June 2018 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) is launching its first magnetic sensors based on TMR technology. This makes the company the world’s first sensor manufacturer to offer magnetic sensors based on all four magnetic technologies: HALL, GMR, AMR and TMR. Infineon will present the new XENSIV™ TLE5501 angle sensor family at the Sensor+Test 2018 fair in Nuremberg (26-28 June). In terms of functional safety, this is a milestone: Infineon is also the first supplier in the market to achieve the highest automotive functional safety grade ASIL D for angle sensors with only one single sensor chip.

The new products are fast analogue TMR-based angle sensors dedicated to automotive applications. Their fields of use range from steering angle applications with the highest functional safety requirements to motors for wipers, pumps and actuators and electric motors in general. They are also ready to be used in industrial and consumer applications like robotics or gimbal.

The TMR technology offers a high sensing sensitivity that comes with a high output voltage realizing output signals of up to 0.37 V/V for all XENSIV TLE5501 products. Unlike other technologies, a TMR-based sensor can be connected directly to the microcontroller without any further amplification, thus saving costs for the customer. Furthermore, TMR shows a very low temperature drift reducing external calibration and compensation efforts. In addition, TMR technology is well known for its low current consumption, which is as low as 2 mA for the XENSIV TLE5501 family.

The new sensor family will be available at two different qualification levels. The TLE5501 E0001 is qualified according to AEC Q100. This version is pin-compatible to the established Infineon TLE5009 but can enable cheaper systems as no additional amplifier is necessary. The other version, the TLE5501 E0002, offers ISO26262-compliant development, achieving ASIL D level with just one single chip. It incorporates decoupled bridges for redundant external angle calculation and offers highest diagnostic coverage as demanded by functional safety regulations.

Availability

Infineon will introduce the XENSIV TLE5501 family to the mass market in August 2018. Further information is available at www.infineon.com/angle-sensors. Samples are available via this webpage from August 2018 onwards.

Infineon at the Sensor+Test 2018

At the Sensor+Test 2018 tradeshow (Nuremberg, Germany, 26-28 June 2018) Infineon is presenting its latest sensor technologies. The company is showing its demos for enabling devices to sense the world at booth 429 in hall 1. Information about the Sensor+Test show highlights is available at www.infineon.com/sensortest.

Information Number

INFATV201806-064

Press Photos

  • With its XENSIV™TLE5501 TMR-based angle sensors Infineon is the first supplier to reach ASIL D in angle sensors with only one sensor chip
    With its XENSIV™TLE5501 TMR-based angle sensors Infineon is the first supplier to reach ASIL D in angle sensors with only one sensor chip
    TLE5501_DSO-8-3

    JPG | 724 kb | 2014 x 2126 px