Edge AI company Imagimob introduces Ready Models – the fastest way to take machine learning to production
Munich, Germany – 6 December 2023 – In line with its mission to offer the best and fastest ways to take smart devices to market, Imagimob, an Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) company, is now launching IMAGIMOB Ready Models. The complete machine learning (ML) solutions are guaranteed to be robust, high-performing, and production-ready for edge devices. Ready Models can be quickly deployed onto existing microcontroller (MCU) hardware, such as PSoC™ 6, without the cost, time, or expertise required for custom development.
“If you look at the Edge AI space right now, you can probably count on one hand how many companies provide off-the-shelf models for any one solution,” said Sam Al-Attiyah, Head of Customer Success at Imagimob. “Our Ready Models are built upon eight years of expertise and thoroughly tested out in the field in different environments, so they are validated in terms of performance. And the fact that we are running them on small edge devices is really unique.”
To ensure the robustness of the Ready Models, Imagimob creates a comprehensive list of different scenarios they can encounter, and then test those scenarios. The models are also tested in different scenarios all over the world to ensure they work with no bias based on specific geographies or ethnicities. Finally, field testing on device allows to test and document realistic model performance in an expected hardware setup. The result of all this is a model that does exactly what customers want it to when it's running in their products.
Imagimob is launching four audio-based Ready Models, including Baby Cry for baby monitors, Siren Detection for pedestrians as well as Coughing Detection and Snoring Detection which are both for wearable devices in the medtech and health sectors. Additional models are currently under development within Audio, Radar, IMU (Inertial Measurement Unit) and Capacitive Sensing.
An easier starting point for new ML journeys
For many companies seeking to upgrade products with smart AI features, up until now, the barriers have been too high. The typical development process for a custom-made ML model not only requires the right software engineering and AI expertise, but also a great investment of time and resources for an extensive development process that spans from collecting, validating, and labeling data, to training models based on that data, deploying them on device, and then testing them in diverse environments to ensure performance expectations are met.
In contrast, IMAGIMOB Ready Models require zero or limited engineering and AI competence to implement. And with all of the development and testing work already put in, they essentially offer a shortcut to the marketplace. “This is a much easier way for companies to begin their ML journeys – they don’t have to make such a big investment to start using it on their edge devices,” said Anders Hardebring, CEO at Imagimob. “Depending on the skillset and expertise in a company, developing a custom model for production typically takes six months to a year. With our Ready Models, they can have new Edge AI features up and running essentially overnight.”
Availability
IMAGIMOB Ready Models are now available for purchase. More information is available at www.imagimob.com/ready-models.
About Imagimob
Imagimob is a fast-growing startup driving innovation at the forefront of Edge AI and tiny machine learning, enabling the intelligent products of the future. Based in Stockholm, Sweden, the company has been serving global customers within the automotive, manufacturing, healthcare, and lifestyle industries since 2013. In 2020, Imagimob launched the platform IMAGIMOB Studio for the swift and easy end-to-end development of Edge AI applications for devices with constrained resources. IMAGIMOB Studio guides and empowers users throughout the entire development journey, resulting in game-changing productivity and faster time-to-market. And with the newly launched Ready Models, Edge AI can be implemented quickly and easily. Tirelessly dedicated to staying on top of the latest research, Imagimob is a market leader within AI and embedded technologies. Since May 2023, Imagimob is part of Infineon.
About Infineon
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The company has around 58,600 employees worldwide and generated revenue of about €16.3 billion in the 2023 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Further information is available at www.infineon.com
This press release is available online at www.infineon.com/press
Information Number
INFCSS202312-035